SF_FLASH_READPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

04.06.070_SF_FLASH_READ

Reading of user data from the flash memory

The function block reads a data set from a data segment in the flash memory and stores this data set beginning at the starting flag defined at input SM. The data contained in the data set were previously stored to the flash memory using the SF_FLASH_WRITE function block.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

Access to the flash memory is only possible using the function blocks SF_FLASH_WRITE, SF_FLASH_DEL and SF_FLASH_READ.

NB blocks are read starting at block BNR within segment SEG and stored starting at address SM.

32 binary data or 16 word data or 8 double word data are read per block.

One block contains 38 bytes:

  • 32 bytes of data

  • 4 bytes for CRC checksum

  • 1 byte as "written" identifier

  • 1 byte for alignment

⮫ Table 1144 “Structure of one of the flash memory segments with user data”

Reading a data set is triggered once by a FALSE/TRUE edge at input EN. If no error occurred while reading the data, output DONE is set to TRUE and the outputs ERR and ERNO are set to FALSE. The data set is stored beginning at the defined start flag SM.

Storing the data set can take several CPU cycles.

If an error occurs during reading, DONE and ERR are set to TRUE and data from SM are equal to 0. The error type is indicated at output ERNO.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

This function block is activated by a positive edge of the input variable EN. During the cycle where the function block notices that the operation is finished (output DONE = TRUE) it will set the output variables only for one cycle. When the function block is called again it will reset the output variables immediately.

Table 1143: FB name: SF_FLASH_READ

Name

Data type

Initial value

Description, parameter values

VAR_INPUT

EN

BOOL

FALSE

Activation of the FB using a positive edge

The following applies:

  • EN = FALSE/TRUE edge: Reading the data set is carried out once.

  • EN = TRUE: The function block is not processed, i.e. it does not change its outputs anymore.

NB

WORD

16#0000

Number of data set blocks (decimal 1 ... 1724)

Input NB is used to specify the number of blocks contained in the data set. 32 byte data or 16 word data or 8 double word data are read per block.

Valid values: 1 ... 1724

Example:

  • SM = ADR(%MW0.0) and NB = 1: Data are stored at %MW0.0 to %MW0.15 (1 block = 16 word data)

  • SM = ADR(%MW0.0) and NB = 2: Data are stored at %MW0.0 to %MW0.31 (2 blocks = 32 word data)

SEG

BYTE

16#00

ID number of the data segment (16#01 or 16#02)

BNR

WORD

16#0000

Starting block number in the flash memory data segment (decimal 0 ... 1723)

SM

DWORD

16#00000000

Destination address for the read data set (address of the first variable where the data are placed)

VAR_OUTPUT

DONE

BOOL

FALSE

Reading procedure is completed (DONE = TRUE)

This output always has to be considered together with output ERR.

The following applies:

  • DONE = TRUE and ERR = FALSE: Reading completed. The data set has been stored beginning at the defined input SM.

  • DONE = TRUE and ERR = TRUE: An error occurred while reading the data set. Output ERNO indicates the error number.

ERR

BOOL

FALSE

Error occurred (data segment could not be read)

This output always has to be considered together with output DONE. The following applies if an error occurred: DONE = TRUE and ERR = TRUE. Output ERNO indicates the error number.

ERNO

WORD

16#0000

Error number⮫ [3].

Output ERNO indicates an error number. This output always has to be considered together with the outputs DONE and ERR.

The SF_FLASH_READ operation may take quite a long time since the safety CPU user program is processed with higher priority. Output ERNO indicates that the function block has started the execution (0x0FFF = BUSY).

During this phase, the outputs ERR and DONE are set to FALSE.

Table 1144: Structure of one of the flash memory segments with user data

Byte:

1 | 2

3 | 4

5 | 6

...

29 | 30

31 | 32

33 ... 36

37

38

Byte offset

Block no.

Word 1

Word 2

Word 3

...

Word 15

Word 16

CRC

Written identifier

Alignment

0

0

38

1

76

2

...

...

65436

1722

65474

1723

Call in ST

READ_FLASH(EN := EN_FLASH_READ,
NB := NB_FLASH_READ,
SEG := SEG_FLASH_READ,
BNR := BNR_FLASH_READ,
SM := SM_FLASH_READ,
DONE => DONE_FLASH_READ,
ERR => ERR_FLASH_READ,
ERNO => ERNO_FLASH_READ);